Syntax
/mmaster_recipe
Recognized by
All recipe programs.
Description
The Master Recipe parameter allows you to specify the master recipe you want to use with a recipe program. The exact function of the parameter depends on the recipe program.
When specified to the... | The program... |
Recipe Builder | Automatically opens the specified master recipe. If the Recipe Builder automatically starts up with the Recipe Operations window, the parameter is ignored. Instead, the Recipe Builder opens a blank, untitled recipe. NOTE: If the Recipe Builder is already running, this parameter is ignored. |
Recipe Download program | Downloads the specified master recipe to the database. |
Recipe Upload program | Uploads the specified master recipe from the database. |