Deleting Recipes

As your needs change, you may find you no longer need certain recipes. When you decide that a specific recipe is not necessary, you can delete it using the Delete command. This command also deletes all files associated with this recipe.

When you select the Delete command, the Delete Recipe dialog box appears. This dialog box has the following controls:

Recipe Name field — enables you to enter the name of the recipe you want to delete.

Recipe list box — displays the available recipes in the current path that you can delete.

Delete button — deletes the specified master and control recipes and their associated files.

To delete a recipe:

  1. On the File menu, click Delete. The Delete Recipe dialog box appears.
  2. Type the name of the recipe you want to delete.

    If you prefer, you can select the recipe to delete by selecting it from the list box. The file you select appears in the Recipe Name field.

  1. Click Delete. A message box appears displaying the following text:

Are you sure want to delete recipe recipe?

NOTE: Do not attempt to delete files from a file server while they are in use. If you do, the Recipe Builder displays an error message box informing you that the files could not be deleted.

See Also

How Do I...