Creating a Sample Recipe

From the steps in the previous subsection, you can obtain most of the information you need to create the recipe. The following table summarizes this information.

Sample Recipe Information

Step

Tagname

Process Value

Verify the fermenter interlock is inactive.

ILK1.F_CV

0

Open the transfer valve to move the wort from the brew kettle to the fermenter.

XCV1F1.F_CV

0

Weigh out 150 pounds of yeast and add to wort.

W16S1.F_CV

150

Set the fermenter temperature to 55 degrees Fahrenheit.

T16F1.F_CV

55

Set the fermenter timer to 132 hours.

K16F1.F_CV

132

With this information, you can now create a recipe for fermenting beer by selecting the appropriate cell in the Recipe Builder spreadsheet and typing the information into it. Press Enter when you finish typing. The following figure shows the sample recipe.

Sample Recipe

You can also enter the tagname of the download interlock into the Recipe Builder. Once defined, the Recipe Builder automatically examines the value of this tagname during a download and if the interlock is inactive, the program downloads the recipe. In the sample recipe, you would enter the tagname ILK1.F_CV for the download interlock. For more information about entering the download interlock, refer to the section Defining the Upload and Download Interlocks.