Selecting an Action

NOTE: You must have a key combination defined before you can select an action.

To select an action with the Multiple Command Script Wizard:

  1. In the iFIX Key Macro Editor main window, click the Run Wizard button. The Multiple Command Script Wizard appears.
  2. Choose a command from the Select Action to Append list. The Expert associated with the command you chose appears.
  3. Complete the Expert with your desired settings and information.
  4. Optionally, repeat steps 2 and 3 if you want to add additional commands to your scripted command sequence.
  5. When you have finished choosing your command sequence, click OK.

To select an action with the Visual Basic Editor:

  1. In the iFIX Key Macro Editor main window, click the VB Editor button. The Visual Basic Editor appears.
  2. Create your custom script in the VB Editor, then click OK.

For more information on the Multiple Command Script Wizard, see The Multiple Command Script Wizard.  For more information on creating custom scripts, see the iFIX Automation Interfaces Help.

See Also