To set a SCADA
server's alarm priority:
- In the iFIX WorkSpace configuration environment, open or create a picture.
- In Classic view, from the Shapes toolbar, click the Data link button.
-Or-
In Ribbon view, on the Insert tab, in the Objects/Links group, click Objects/Links, and then click Datalink.
-Or-
If the Toolbox is enabled, click the Datalink button on the Toolbox.
The cursor changes to a plus sign.
- Click and drag the mouse to define the size of the Data link. The Datalink dialog box appears.
- In the Source field, enter the data source Fix32.node.System.A_SACPR.
- From the Type drop down menu in the Data Entry area, select In-Place.
- Complete the remainder of the Datalink dialog box.
- Switch to the run-time environment and enter the SCADA server's alarm priority.
See Also