Deleting an Animation in the Basic Animation Dialog Box
To delete an
animation using the Basic Animation dialog box:
- In the iFIX WorkSpace, select Animations from the object's right-click menu. The Basic Animation dialog box appears. If a property contains an animation, the check box is selected.
- Clear the check box to delete the animation.
Based on your User Preferences settings, you may be prompted to acknowledge this action by clicking Yes. To configure whether or not you are prompted upon deleting an animation, modify the Prompt on Delete option in the Picture Preferences tab of the User Preferences dialog box.
IMPORTANT: To delete all animations you configured in the Advanced Animations dialog box, clear the Advanced Animations check box. If you have assigned multiple animations from the Advanced Animations dialog box, be aware that you will be deleting all of those animations. If you have multiple animations assigned in the Advanced Animations dialog box, it is recommended that you delete them separately within the Advanced Animations dialog box itself.