Accessing the Animation Dialog Boxes

iFIX provides the following options for configuring Animations:

  • Experts – In the iFIX WorkSpace, select the appropriate Expert from the Experts toolbar, or the Task Wizard (Classic or Ribbon views) or on the Tools tab, in the Animations group, Animations  list (Ribbon view). If the Toolbox is enabled, click the button on the Toolbox.
  • Basic Animation dialog box – In the iFIX WorkSpace, double-click an object or select Animations from the right-click menu. This dialog box contains many commonly used animations. For a listing of all animations available to an object, use the Advanced Animations dialog box.
  • Advanced Animations dialog box – Click the Configure button on the Basic Animation dialog box; or, if configured, the Advanced Animations dialog box appears when you double-click an object in the iFIX WorkSpace or select Animations from the right-click menu.

NOTE: To configure the Advanced Animations dialog box to always appear when you double-click an object or select Animations from the right-click menu, clear the Always Show Basic Animation dialog box option on the Picture Preferences Tab of the User Preferences dialog box.

See Also