Setting the Fade Type of an Object
To set the fade
type of an object:
- In the iFIX WorkSpace, right-click the object, point to Color, and choose Fade.
- In the Fade Type area, select the fade type you want to apply to the object.
- Or -
If the object already has a gradient style applied to it, right-click the object, point to Fade Type and choose the fade type you want to apply.
NOTE: Selecting a fade type in the Select FadeColor dialog box automatically sets the object's fill style to Gradient, regardless of the setting in the User Preferences dialog box.
See Also