To complete a
range data conversion:
- In the iFIX WorkSpace, double-click the object you want to modify. The Basic Animation dialog box appears.
- Click Configure. The Advanced Animations dialog box appears.
- Click the tab containing the property you want to change, and select the Animate check box next to that property.
- From the Data Conversion list, select Range.
- In the Minimum Input and Minimum Output fields, enter the minimum input and output values, as needed.
- In the Maximum Input and Maximum Output fields, enter the maximum input and output values, as needed.
- If you want the selected object to read a value from the data source when the picture opens, select the Fetch Input Range on Open check box.
- If you want to perform an animation on an object in its current position, not in the absolute position specified by the logical unit or postscript point value in the Minimum Output field, select the Use Offset check box.
See Also