Completing a Format Data Conversion

To complete a format data conversion:

  1. In the iFIX WorkSpace, double-click the object you want to modify. The Basic Animation dialog box appears.
  2. Click Configure. The Advanced Animations dialog box appears.
  3. Click the tab containing the property you want to change, and select the Animate check box next to that property.
  4. From the Data Conversion list, select Format.
  5. In the Type field, specify whether you want to write data to the database. In-Place allows the user to write to the database.
  6. Select the Confirm check box if you want operators to confirm each entry they make.
  7. From the Justify list, select how to justify the data on the screen.
  8. From the Type list, select the type of data.
  9. If the data type is alphanumeric, enter the number of lines to display in the Lines field and the number of characters per line in the Chars/Line field. If the data type is numeric, enter a value of 0 to 7 in the Whole Digits field and 0 to 5 in the Decimal field.
  10. Select the Raw Format check box if you want to display data in its raw format.

See Also