Changing Your Window Size

The window size is always defined as a percentage of the screen. By sizing a window by the percentage of the screen, iFIX scales your picture while maintaining its coordinate system and displays the picture with its original aspects regardless of the monitor's resolution on which it is viewed. Both the Window Width and Window Height must be within 0-100 percent.

To change your window size:

  1. In Classic view, in the iFIX WorkSpace, on the Edit menu, click Picture.

-Or-

In Ribbon view, on the Home tab, in the Editing group, click Properties, and then click Picture.

  1. In the Window Width field, enter a picture width as a percentage.

NOTE: Be careful when entering a percentage as its meaning is different for each coordinate system. For more information on percentages for both coordinate systems, refer to the Controlling a Picture's Magnification section.

  1. In the Window Height field, enter a picture height as a percentage.
  2. Click the Apply button to view the change.
  3. Continue to adjust the percentages and apply the changes until you have the picture as you want it to be.
  4. Click the OK button to save the window settings.

See Also