Adding Data Links Using the Data Entry Expert
To add a data
link using the Data Entry Expert:
- In the iFIX WorkSpace, double-click a Data link.
- In the Data Entry Type field of the Datalink dialog box, select None and click OK.
NOTE: If you set the Data Entry Type field to In-Place, unexpected results may occur.
- In Classic view, on the Standard toolbar, click the Task Wizard button.
-Or-
In Ribbon view, on the Tools tab, in the Tasks/Experts group, click the Tasks/Experts dialog box launcher.
- From the Task Categories list, select Data Entry Expert and click Perform Task.
- In the Data Source field, enter a data source for the data link. To use the Expression Builder, click the Browse button.
- In the Choose Data Entry Method area, select the appropriate data entry option.
- Set the values of the fields corresponding to the data entry method you chose.
- Click OK.
See Also