Modify Area Dialog Box
The Modify Area dialog box displays the following items:
Available
Lists the alarm areas that are currently available. To filter alarms by alarm area, select the area(s) from this list and select the In or Not In option button.
In
Allows you to filter alarms by the alarm areas that are currently selected in the Available list. When this option is selected, the Alarm Summary object displays only those alarms from the selected alarm areas.
Not In
Allows you to filter alarms by the alarm areas that are currently selected in the Available list. When this option is selected, the Alarm Summary object ignores all alarms from the selected alarm areas.
Add Area Not Currently in List Edit Box
Allows you to add an alarm area name to the Available list, if it does not appear by default. Enter the alarm area name in this field and click Add to add it to the list.
Add Button
Allows you to add an alarm area name to the Available list, if it does not appear by default. Enter the alarm area name in the Add Area Not Currently In List field and click this button to add it to the Available list.