To add a Dynamo
object to a Dynamo Set:
- In the iFIX WorkSpace, open an existing Dynamo Set or create a new one.
- Drag-and-drop or copy and paste the Dynamo object you created with the Build Dynamo Wizard into the Dynamo Set.
If more than one object is selected, the Add Object to Dynamo Sets dialog box appears.
- If the Add Object to Dynamo Sets dialog box appears, select the Create a New Master Dynamo option and click OK. The Dynamo is added to the set as a Master Dynamo.
Each new Dynamo object that you add to the set becomes a Master Dynamo.
- Save the Dynamo Set.