General Tab - Alarm Summary Configuration Dialog Box

The General tab of the Alarm Summary Configuration dialog box contains the following item:

Description

Allows you to enter a description for the Alarm Summary object.

Alarm Summary Column Headers

Displays the font selected for the column headings in the Alarm Summary object. Only the font name appears in this field. Click the browse (...) button to change the font name, style, size, or script.

After you select a new font and click Apply or OK, the font gets applied to the Alarm Summary object – in both configure and run mode. If the font is larger than the area allowed, the height of the area is adjusted.

Browse (...) Button 1

Click to select a font name, style, size, and script for the column headings in the Alarm Summary object.

Status Bar

Displays the font selected for the status bar in the Alarm Summary object. Only the font name appears in this field. Click the browse (...) button to change the font name, style, size, or script.

After you select a new font and click Apply or OK, the font gets applied to the Alarm Summary object – in both configure and run mode. If the font is larger than the area allowed, the height of the area is adjusted.

Browse (...) Button 2

Click to select a font name, style, size, and script for the text in the status bar of the Alarm Summary object.

How Do I...