Dynamo Updater – Update Behavior Dialog Box

The Dynamo Updater – Update Behavior dialog box displays the following items:

Data Source Adjustments

The Data Source Adjustments area lets you specify how the Dynamo Updater should reconcile a data source mismatch between a Master Dynamo and Dynamo Instance. Select one of the following options:

  • Update the Dynamo, and use Master Dynamo data sources – If you want to update mismatched Dynamo Instances, but do not want to apply any of the data sources from the Dynamo Instance. This option uses all data sources from the Master Dynamo, and no data sources from the Dynamo Instance.
  • Update the Dynamo and try to match up the Data SourcesIf you want to update mismatched Dynamo Instances using data sources from the Dynamo Instance and a best guess matching algorithm.

For example, if a Master Dynamo object contains only one data source (user prompt) based on an animation, but a previous version (an instance of that Dynamo) includes three data sources based on animations, a best guess match is made. For the best guess, iFIX decides which one of the three data sources to use in the instance, and a report is generated based on your settings.

If the object type differs between the Master Dynamo and the Instance, there is no attempt to update the data sources in the animation for that object.

  • Do not update Dynamo – If you only want to view a report of mismatched Dynamos and make no actual updates.

Apply

Applies the selected adjustment option to a single Dynamo object in the update.

Apply to All

Applies the selected adjustment option to all Dynamo objects in this update.

How Do I...