Dynamo Updater Dialog Box
The Dynamo Updater dialog box displays the following items:
Quick Dynamo Report
Item |
Description |
Dynamo Instances Mismatched With Revision Of Master Dynamo – List Box |
Displays the Dynamo Instances that were found to be a different revision from their associated Master Dynamo. This list is generated from the Quick Dynamo Updater dialog box or the Dynamo Updater Wizard dialog box. |
Dynamo Instances Mismatched With Revision Of Master Dynamo – Table |
Displays the name, object description, dynamo description, revision, file name, and full name of the Dynamo Instance and Master Dynamo associated with the Dynamo selected in the mismatch list. |
Update Dynamo Instances
Item |
Description |
Update Behavior |
Displays the currently selected behavior that the Dynamo Updater should use when the number of data sources does not match between a Master Dynamo and Dynamo Instance. |
Modify |
Click the Modify button to change the Update Behavior. |
Maintain Size |
Select to retain the current size of the Dynamo Instance. |
Maintain Captions |
Select to retain existing captions for all Dynamo Instances. |
Update Progress Status |
The Update Progress Status bar graphically displays the progress of the Dynamo Update process. |
Update Progress Status – Log Display |
Displays the date, time, and status of each Dynamo Instance and Master Dynamo modification attempted as part of the automated Dynamo Update process. |
Run Update
Launches the update process, which reconciles the revision differences between associated Dynamo Instances and Master Dynamos. Updates are made based on the Update Behavior setting.
NOTES:
- While the update process is running, the Run Update button changes to a Cancel Update button, allowing you the option of canceling the update while it is in progress.
- The Dynamo Updater does not support dynamos with Enhanced Charts.