The User Preferences dialog box contains several additional properties you can apply to your pictures. To access them click the Picture Preferences tab. The following properties are available in the right column of the Properties area:
- Highlight Timeout Interval – When Click and Stick is enabled, this time period defines how long before the highlight around an object disappears when it is not selected.
- Grid Interval – When the grid is enabled, this interval (entered in pixels) determines the distance between the dots in the grid.
- Using Click and Stick – Click and Stick allows you to view which objects can be selected, highlighted, or modified at run-time. As the mouse moves over an object, a single highlighted box clicks around the object if it is selectable. If the object is highlighted, use the mouse to select or stick the object and it becomes the current object. To enable or disable Click and Stick, select or deselect the Click and Stick Enabled check box.