You can also create pictures with no title bars. This is a particularly helpful feature when you want to view your pictures as is in your operator display. The following figure illustrates a picture without a title bar.
Picture without a Title bar
You cannot tile or cascade a picture without a title bar.
If you want to create a full screen picture without a title bar make sure that you deselect the Title bar check box.
To create a full screen picture without
a title bar:
- In Classic view, on the WorkSpace menu, click User Preferences.
-Or-
In Ribbon view, on the Home tab, in the WorkSpace group, click Settings, and then click User Preferences.
- Click the Picture Preferences tab.
- Deselect the Titlebar check box.
- Click OK.
NOTE: If you intend to autoscale pictures created without titlebars, the picture must be started titleless.
There are many additional style options for the picture window. For more information on these window properties, refer to the Planning Your Pictures section.