Column Tab - Alarm Summary Configuration Dialog Box

The Column tab of the Alarm Summary Configuration dialog box displays the following items:

Columns Area

Item

Description

Available Columns

Lists the columns that are available to be added to the Alarm Summary object.  To add a column, select the column name and click Add. The name of the column appears in the Selected Columns list, and appears in the Alarm Summary object at run-time.

Add

Allows you to add the currently selected column in the Available Columns list to the Alarm Summary object.

Remove

Allows you to remove the currently selected column in the Selected Columns list from the Alarm Summary object.

Selected Columns

Lists the columns that appear in the Alarm Summary object at run-time. To remove a column from the list, select the column name and click Remove. To change the order of the columns, select the column name and use the up and down arrows to move the column to the desired positon.

Up

Moves the selected column name up in the Selected Columns list. This has the effect of moving the column to the left in the Alarm Summary object at run-time.

Down

Moves the selected column name down in the Selected Columns list. This has the effect of moving the column to the right in the Alarm Summary object at run-time.

User Definable Columns

Item

Description

User Defined Field 1

Allows you to assign a different ASCII (A_) block field to the User Defined Field 1 column. The default field is A_CUALM. This field is available only if the User Defined Field1 column has been added to the Selected Columns list.

<> (first instance)

Changes the ASCII (A_) block field that is represented by the User Defined Field 1 entry in the Selected Columns list to the field currently entered in the User Defined Field.

User Defined Field 2

Allows you to assign a different ASCII (A_) block field to the User Defined Field 2 column. The default field is A_AUTO. This field is available only if the User Defined Field2 column has been added to the Selected Columns list.

<> (second instance)

Changes the ASCII (A_) block field that is represented by the User Defined Field 2 entry in the Selected Columns list to the field currently entered in the User Defined Field 2 field.

User Defined Field Name 1

Specifies the text displayed in the header of the Alarm Summary object's User Defined Field1 column.  The text you specify cannot match the text of any existing column header, including the text used in the User Defined Field2 column header.  The maximum length of this name is 50 characters.  

User Defined Field Name 2

Specifies the text displayed in the header of the Alarm Summary object's User Defined Field2 column.  The text you specify cannot match the text of any existing column header, including the text used in the User Defined Field1 column header.  The maximum length of this name is 50 characters.  

How Do I...