Setting the Alarm Foreground Color
To select the
alarm foreground color:
- In the iFIX WorkSpace, double-click the Alarm Summary object. The Alarm Summary Configuration dialog box appears.
- Select the Color tab.
- Next to each alarm priority or status, double-click the color. The Select Color dialog box appears.
- Select a new color for the alarm status or priority and then click OK.
- Repeat the previous two steps for each row in the Foreground Alarm Color area.
- If the Unacknowledged Alarm Color option is enabled, double-click the color next the field to define the unacknowledged alarm color.
- Click Apply.
See Also