Add Date Last Dialog Box
The Add Date Last dialog box displays the following items:
Operator
Item |
Description |
= |
Allows you to configure the Alarm Summary object to display only those alarms that are equal to the value of the field to the right. For example, if the equal operator is used in conjunction with the Time In field, and the value in the Time In field is 10:00:00, then the Alarm Summary object will display only those alarms that first occurred at 10:00:00. |
< > |
Allows you to configure the Alarm Summary object to display only those alarms that are not equal to the value of the field to the right. For example, if the not equal operator is used in conjunction with the Time In field, and the value in the Time In field is 10:00:00, then the Alarm Summary object will display all alarms that did not first occur at 10:00:00. |
> |
Allows you to configure the Alarm Summary object to display only those alarms that are greater than the value of the field to the right. For example, if the greater than operator is used in conjunction with the Time In field, and the value in the Time In field is 10:00:00, then the Alarm Summary object will display only those alarms that first occurred after 10:00:00. |
>= |
Allows you to configure the Alarm Summary object to display only those alarms that are greater than or equal to the value of the field to the right. For example, if the greater than or equal to operator is used in conjunction with the Time In field, and the value in the Time In field is 10:00:00, then the Alarm Summary object will display all alarms that first occurred at or after 10:00:00. |
< |
Allows you to configure the Alarm Summary object to display only those alarms that are less than the value of the field to the right. For example, if the less than operator is used in conjunction with the Time In field, and the value in the Time In field is 10:00:00, then the Alarm Summary object will display only those alarms that first occurred before 10:00:00. |
<= |
Allows you to configure the Alarm Summary object to display only those alarms that are less than or equal to the value of the field to the right. For example, if the less than or equal to operator is used in conjunction with the Time In field, and the value in the Time In field is 10:00:00, then the Alarm Summary object will display all alarms that first occurred at or before 10:00:00. |
Date Last
The date when the block last generated the alarm – used as a condition to filter alarms.