Using the Security Synchronizer Automation Interface

The Security Synchronizer program is a background task that you use with command line parameters to execute the security synchronization process.

You can also program the synchronization process using the SecuritySynchronizer Automation object. This object provides the properties and methods you need to synchronize iFIX security with your Windows security configuration. You have the ability to write custom applications or scripts that automate how and when the security synchronization process executes.

For a description of the SecuritySynchronizer object and the properties and methods available through it, see the iFIX Automation Interfaces Help file.