Setting Passwords to Expire

One of the benefits of using iFIX with Windows security is that you can set Windows passwords to expire.

To configure the local password expiration policy:

  1. In the Control Panel, from the Administrative Tools folder, select the Local Security Policy.
  2. From the Local Security Settings window, select Account Policies.
  3. From the Account Polices folder, select Password Policy.
  4. On the right-side of the window, double-click the Maximum password age.
  5. Set the number of days after which passwords expire.
  6. Click OK.

See Also

How Do I...