Built in iFIX Groups that Appear in Proficy Authentication
By default, built in iFIX security groups are added to Proficy Authentication. The following table describes these groups in iFIX and in Proficy Authentication, and the associated iFIX application features that are associated with each group.
NOTE:Once you delete a group in iFIX, Proficy Authentication will not recognize that the group is deleted in iFIX. So the Proficy Authentication users in that group will not have the permission to use the associated iFIX application features.
Proficy Authentication Group | iFIX Security Group | Description | iFIX Application Features |
---|---|---|---|
scada.ifix_shared_IFIX_PROFICY_AUTH_ADMIN |
IFIX_PROFICY_AUTH_ADMIN |
This group allows access to all iFIX application features. So, any Proficy Authentication user who is a member of this group will have privileges similar to a native iFIX ADMIN user (except the access to security areas). Proficy Authentication users who want to directly log in to iFIX can use this group. NOTE: This group is not available by default when you upgrade from iFIX 6.1 or 6.5. You must manually create this group with all the iFIX application features as needed. For more information on how to create groups, refer to the section Creating a Group Account to Proficy Authentication. |
|
scada.ifix.shared.APPLICATION_DESIGNER |
APPLICATION_DESIGNER |
This group allows a user to access Configuration Hub and provides use of iFIX features such as iFIX connection, database, and model management. It does not include support for the new features introduced in Configuration Hub 2022 (for the SCU and iFIX Security Configuration). NOTE: This group is not available by default when you upgrade from iFIX 6.1 or 6.5. You must manually create the group with all the iFIX application features as needed. If upgrading from iFIX 2022, this group does appear but does not have the Security Configuration or System Configuration features included for the new project management and deployment features. IMPORTANT: If you want to create a new iFIX security group that has support for the all the new features, at a minimum, you need to include the following features:
For information on how to create groups in Proficy Authentication see: Creating a Group Account to Proficy Authentication. |
|
scada.ifix.shared.OPERATORS |
OPERATORS | This group provides run mode only access for a user in iFIX. |
|
scada.ifix.shared.SUPERVISORS |
SUPERVISORS | This group provides access to WorkSpace run and configure mode, as well as access to background task exit, iFIX system shut down, and iFIX system user login. |
|
scada.project.admin | N/A | This group allows the Proficy Authentication user access to the Projects panel and to the Deploy operations from Configuration Hub. | N/A |