Working with the Pop-up Menu

In addition to the properties you can configure, the spreadsheet lets you right-click any row, column, or cell to display a menu containing a list of frequently-accessed commands. These commands are identical to commands you can access from the menu bar. For example, Cut on the pop-up menu is identical to Cut on the Edit menu. Similarly, Add Block on the pop-up menu is identical to Add on the Blocks menu.

 

See Also