Using Visual Basic for Applications (VBA) or the Scheduler, you can adjust database values, place blocks on scan or off scan, change a block's mode, or launch a script based on a value change or an alarm. For example, using a time-based schedule, you could set the values of a dozen blocks prior to the manufacture of your product or you could automatically ramp a value based on an event (such as a valve closing). Likewise, you could write a script to monitor the value of a block and, when an alarm occurs, open a diagnostic picture. For more information on using these features, refer to the Writing Scripts and Mastering iFIX manuals.