Changing the Order of Solve

You can change the order of solve by exporting the database and editing the export file. Database Manager exports primary blocks in the order SAC scans all primary blocks. This results in all Analog Input blocks appearing first in the export file, followed by all Analog Output blocks, and so on. Once the primary block types are exported, Database Manager exports the secondary blocks.

For example, using the blocks in the Sample Calculation Chain figure, you can ensure SAC scans AI1 after AI2 and AI3 as follows:

  1. Export the database.
  2. Locate AI2's and AI3's entries in the export file.
  3. Move both entries to the start of the file.
  4. Save the export file and import it into an empty database.

For more information about completing these tasks, refer to the sections Exporting Databases and Importing Databases.

 

See Also