You can enable specific operator and run-time properties in the Alarm
Summary object. The operator properties enable operators to work interactively
with the object by acknowledging, deleting, filtering, and sorting alarms
at run-time. The run-time properties control time intervals used by the
object. The following two tables summarize the operator and run-time properties
you can configure.
Alarm Summary Operator Properties
The property...
|
Lets operators...
|
Allow Alarm Acknowledgement
|
Acknowledge alarms with the Alarm Summary object.
|
Allow Alarm Deletion
|
Delete alarms from the Alarm Summary object. Unlike
the manual deletion option configured in the SCU, the deleted alarms do
not need to be acknowledged first.
|
Allow Run Time Configuration
|
Change the filter and sort properties of the Alarm
Summary object at run-time.
|
Enable Column Quick Sort
|
Sort alarms by clicking a column heading.
|
Display Right Mouse Menu
|
Right-click the mouse to display a list of commands
to acknowledge, filter, sort, delete, and pause alarms.
|
Alarm refresh rate
|
The Alarm Summary object examines the Alarm Summary
queue for new alarms.
|
Data refresh rate
|
The Alarm Summary object updates the alarm values
currently displayed.
|
Blink rate
|
An alarm flashes when you enable blinking for it.
|
Selection Timeout
|
A row in the spreadsheet remains selected. Typically,
the spreadsheet automatically scrolls while receiving new alarms. When
you select an alarm from the spreadsheet, the scrolling pauses until the
selection timeout expires.
|
NOTE: You can also
acknowledge, delete, filter, and sort alarms in the Alarm Summary object
using an Expert or a script. For more information on completing these
tasks using an Expert, refer to the Creating Pictures manual. To learn about the
iFIX automation interface, refer to the Writing Scripts manual.
See Also
How Do I...