Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / WriteLine Method / WriteLine(Object) Method
Value to write.


In This Topic
    WriteLine(Object) Method
    In This Topic
    Writes the supplied value to System.Diagnostics.Trace and to all registered listeners such as file and/or console.
    Syntax
    Public Overloads Shared Sub WriteLine( _
       ByVal value As System.Object _
    ) 
    public static void WriteLine( 
       System.object value
    )
    public:
    static void WriteLine( 
       System.Object^ value
    ) 

    Parameters

    value
    Value to write.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also