Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / TraceError Property


In This Topic
    TraceError Property
    In This Topic
    Gets whether tracing of error messages to file is configured, level set to Error, Warning, Info or Verbose.
    Syntax
    Public Shared ReadOnly Property TraceError As System.Boolean
    public static System.bool TraceError {get;}
    public:
    static property System.bool TraceError {
       System.bool get();
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also