Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Tracer Class / Finalize Method


In This Topic
    Finalize Method
    In This Topic
    Closes the file stream, if any, and re-registeres it for garbage collection.
    Syntax
    Protected Overrides Sub Finalize() 
    protected override void Finalize()
    protected:
    void Finalize(); override 
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also