Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnPublishGetDestinationServer Method
Indication of how the request was processed.
Destination Historian server name.


In This Topic
    OnPublishGetDestinationServer Method
    In This Topic
    Invoked by the remote server to transmit the requested destination server name.
    Syntax
    Public Sub OnPublishGetDestinationServer( _
       ByVal status As Status, _
       ByVal destinationServer As System.String _
    ) 
    public void OnPublishGetDestinationServer( 
       Status status,
       System.string destinationServer
    )
    public:
    void OnPublishGetDestinationServer( 
       Status status,
       System.String^ destinationServer
    ) 

    Parameters

    status
    Indication of how the request was processed.
    destinationServer
    Destination Historian server name.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also