Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnClosing Method
Event source.
Event data.


In This Topic
    OnClosing Method
    In This Topic
    Invoked when the connection object first enters the closing states.
    Syntax
    Protected Sub OnClosing( _
       ByVal sender As System.Object, _
       ByVal e As System.EventArgs _
    ) 
    protected void OnClosing( 
       System.object sender,
       System.EventArgs e
    )
    protected:
    void OnClosing( 
       System.Object^ sender,
       System.EventArgs^ e
    ) 

    Parameters

    sender
    Event source.
    e
    Event data.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also