Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / Disconnect Method


In This Topic
    Disconnect Method
    In This Topic
    Disconnect from a Historian server.
    Syntax
    Public Sub Disconnect() 
    public void Disconnect()
    public:
    void Disconnect(); 
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also