Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / MultiField Class / NumberOfFields Property


In This Topic
    NumberOfFields Property
    In This Topic
    Number of fields in this MultiField type .
    Syntax
    Public Property NumberOfFields As System.Integer
    public System.int NumberOfFields {get; set;}
    public:
    property System.int NumberOfFields {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also