Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / MultiField Class / LastModifiedUser Property


In This Topic
    LastModifiedUser Property (MultiField)
    In This Topic
    The user name of the user whp modified the MultiField type last.
    Syntax
    Public Property LastModifiedUser As System.String
    public System.string LastModifiedUser {get; set;}
    public:
    property System.String^ LastModifiedUser {
       System.String^ get();
       void set (    System.String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also