Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IntegerCriteria Class / MinDoubleInteger Property


In This Topic
    MinDoubleInteger Property
    In This Topic
    Syntax
    Public Property MinDoubleInteger As System.Integer
    public System.int MinDoubleInteger {get; set;}
    public:
    property System.int MinDoubleInteger {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also