Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IAlarms Interface / Restore Method


In This Topic
    Restore Method
    In This Topic
    This provides the functionality to restore alarms and events from a bacup file.
    Syntax
    Sub Restore( _
       ByVal restoreFileName As System.String _
    ) 
    void Restore( 
       System.string restoreFileName
    )
    void Restore( 
       System.String^ restoreFileName
    ) 

    Parameters

    restoreFileName
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also