Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / HistorianFault Class / Status Property


In This Topic
    Status Property (HistorianFault)
    In This Topic
    An error status underlying the fault.
    Syntax
    Public Property Status As Status
    public Status Status {get; set;}
    public:
    property Status Status {
       Status get();
       void set (    Status value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also