Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Field Class / Name Property


In This Topic
    Name Property (Field)
    In This Topic
    The name of the individual field
    Syntax
    Public Property Name As System.String
    public System.string Name {get; set;}
    public:
    property System.String^ Name {
       System.String^ get();
       void set (    System.String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also