Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / EnumeratedSetState Class / EnumeratedSetState Constructor


In This Topic
    EnumeratedSetState Constructor
    In This Topic
    Default Constructor. Initialize the states and necessary variables
    Syntax
    Public Function New()
    public EnumeratedSetState()
    public:
    EnumeratedSetState();
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also