Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / EnumeratedSetStateName Class / ReservedForFuture Property


In This Topic
    ReservedForFuture Property
    In This Topic
    Reserverd for LanguageId in the future.
    Syntax
    Public Property ReservedForFuture As System.Integer
    public System.int ReservedForFuture {get; set;}
    public:
    property System.int ReservedForFuture {
       System.int get();
       void set (    System.int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also