Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataStore Class / IsSystem Property


In This Topic
    IsSystem Property
    In This Topic
    Whether the data store is marked as system store
    Syntax
    Public Property IsSystem As System.Boolean
    public System.bool IsSystem {get; set;}
    public:
    property System.bool IsSystem {
       System.bool get();
       void set (    System.bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also