Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataStore Class / IsDefault Property


In This Topic
    IsDefault Property
    In This Topic
    Whether the data store is marked as default store (used as default data store for tags adds, and archive related operations)
    Syntax
    Public Property IsDefault As System.Boolean
    public System.bool IsDefault {get; set;}
    public:
    property System.bool IsDefault {
       System.bool get();
       void set (    System.bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also