Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataSet Class / TotalSamples Property


In This Topic
    TotalSamples Property
    In This Topic
    The total number of data samples for all tags.
    Syntax
    Public ReadOnly Property TotalSamples As System.Integer
    public System.int TotalSamples {get;}
    public:
    property System.int TotalSamples {
       System.int get();
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also