Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / Username Property


In This Topic
    Username Property (ConnectionProperties)
    In This Topic
    A name of a user account with access to the server. If unset the current Windows user is used for authentication.
    Syntax
    Public Property Username As System.String
    public System.string Username {get; set;}
    public:
    property System.String^ Username {
       System.String^ get();
       void set (    System.String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also