Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / ReliableSessionEnabled Property


In This Topic
    ReliableSessionEnabled Property
    In This Topic
    Whether to enable reliable sessions. Default value is false.
    Syntax
    Public Property ReliableSessionEnabled As System.Boolean
    public System.bool ReliableSessionEnabled {get; set;}
    public:
    property System.bool ReliableSessionEnabled {
       System.bool get();
       void set (    System.bool value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also