Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ConnectionProperties Class / OpenTimeout Property


In This Topic
    OpenTimeout Property
    In This Topic
    Maximum amount of time to attempt to open a connection before timing out. Default value is 1 minute.
    Syntax
    Public Property OpenTimeout As System.TimeSpan
    public System.TimeSpan OpenTimeout {get; set;}
    public:
    property System.TimeSpan OpenTimeout {
       System.TimeSpan get();
       void set (    System.TimeSpan value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also