Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / CalculatedQuality Class / CalculatedQuality Constructor / CalculatedQuality Constructor(Single)
A percent value to represent.


In This Topic
    CalculatedQuality Constructor(Single)
    In This Topic
    Constructor.
    Syntax
    Public Function New( _
       ByVal percent As System.Single _
    )
    public CalculatedQuality( 
       System.float percent
    )
    public:
    CalculatedQuality( 
       System.float percent
    )

    Parameters

    percent
    A percent value to represent.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also